Změna jazyka :
With the RM-no camber and GRM-no camber machines, Otto Bihler Maschinenfabrik GmbH & Co. KG has developed the fastest servo stamping and forming machines in the world. Their central feature is a new drive and control concept for the moving spindle. The energy chain with chainflex® cable from igus®, supplied as pre-assembled, ready-to-install "readychains", takes care of the energy supply.
"As the arrangement of the units is not fixed, the energy supply system must be very flexible. Because the space required in or on the machine is limited, the energy supply system must not take up too much installation space. And during punching and bending, pointed and sharp punching residues can occur at any time, which can block the energy chain or damage the cable."
Dipl.-Ing. Paul Maldoner, Head of Machine Development at Bihler, on the requirements for the energy supply system
Osobne:
Pondelok až piatok: 7:00 – 15:00
Online:
Pondelok až piatok: 7:00 – 15:00