Změna jazyka :
Smart igus® e-chain® reliably transport energy, data and media in highly dynamic applications
Moving driving simulators have been used in the German automotive industry for 35 years. The world's most modern driving simulator now boasts the following key data: 2.2 MW of electric drive power, "22 tonnes of agility" and a total value of over 25 million euros.
In the end, the latest generation of e-chain series P41.80 and new chainflex cables were used, which meet all EMC safety requirements as well as standards and directives such as UL, VDE, CSA, Profibus etc. As the existing guide trough was also specially manufactured and adapted to the tight installation space ten years ago and was still in very good condition, those responsible decided to replace only the damping profiles. In the new P41.80 system, the upper and lower run are offset one above the other. This ensures smoother running and ideal noise insulation. In addition to comb-like autoglide bars, the system also has tribologically optimized plastic rollers, which significantly increase the durability of the chains. With this solution, we were able to offer our customer everything from a single source: from project planning, delivery and installation through to maintenance.
Our new brochure shows you everything at a glance
Topic overview:

Osobne:
Pondelok až piatok: 7:00 – 15:00
Online:
Pondelok až piatok: 7:00 – 15:00