Změna jazyka :
Discover all our test reports on the durability tests for our bus cables here.
A display on a machine is literally the control centre where every function of a machine tool is set and controlled. These operating units are often supplied with Ethernet cables to enable fast data transfer in real time. It has proven to be a good idea, especially for large systems, to make this control centre mobile and even linearly movable. A reliable cable is now required here in order to be able to reliably map the recurring movements.

The aim of the test was to determine the service life of the chainflex® bus cable in a radius of 100 mm with a travel of up to 7 metres. The requirement for this Ethernet cable is to ensure reliable data transmission over the longest possible service life despite constant movement.
The quality requirement in combination with a small bend radius is particularly prevalent in industrial machines and applications that have to process a large amount of data. In addition, small installation spaces are often a major challenge for the longevity of the cable.

The bus cable shown here is frequently used in applications where fast handling is required. Short cycle times and the flexibility of handling systems are very important here. This means that the cables used must be able to withstand the highest demands. One example of this is the food industry. Fast handling robots must combine maximum precision, short cycle times and low weight.

The CFROBOT8.045 cable is very often used in automotive production, for example in moving measuring units mounted on the 6th axis of the robot. There they move to inspection points and carry out analyses for quality assurance in production. For this purpose, the cables that transport the sensitive Ethernet signal are twisted a great deal. For such tasks, 100% reliability on the robot counts.

Storage and retrieval machines are typical examples of applications in which high tensile strain is exerted on the individual components, as they are used for the automated loading of high-bay warehouses. The bus cable CFSPECIAL.182.045 for Ethernet CAT5e was specially developed for this sector and can withstand the forces due to the aramid braiding in the outer jacket, trade show. Therefore, this cable is the safe variant for such and other suspended applications.

The CFROBOT8.045 cable is very often used in automotive production, for example in moving measuring units mounted on the 6th axis of the robot. There they move to inspection points and carry out analyses for quality assurance in production. For this purpose, the cables that transport the sensitive Ethernet signal are twisted a great deal. For such tasks, 100% reliability on the robot counts.

Osobne:
Pondelok až piatok: 7:00 – 15:00
Online:
Pondelok až piatok: 7:00 – 15:00